Cancel
Showing results for 
Search instead for 
Did you mean: 

Bottleneck Case

Experimenter
Experimenter

Does anyone have a bottleneck case to solve using plant simulation? thanks

3 REPLIES 3

Re: Bottleneck Case

Siemens Phenom Siemens Phenom
Siemens Phenom
Yes, ... that´s daily business for most of the guys here!

Regards

Always consider using the AttributeExplorer!

Re: Bottleneck Case

Experimenter
Experimenter

i need a case but i can't find..can you send me a case so i can solve it, or do you know where can i find one? thanks

Re: Bottleneck Case

Phenom
Phenom

I would recommend picking up any simulation model you have already made and do a Bottleneck analysis. There are no special requirements for a model in order to do it.

 

 If you don't have anything yet, maybe just put 5 processes in a series production and give them different processing times and see what you can do to improve the output keeping the same rate of input from the source.

 

See 'Bottleneck Analyzer' in help.

Also see Start Page> Small Examples> Tools>Wizards>Bottleneck Analyzer

 

You can also try to find some exercises in the book by Steffen Bangsow.