Cancel
Showing results for 
Search instead for 
Did you mean: 

Broker in Experiment Manager

Experimenter
Experimenter

Hi,

 

Do you have an idea how to change Broker from eg. B1 to B2 in SingleProc1 using experiment manager?

I'm looking for something like this:

    Input Values

    root.SingleProc1.imp.BrokerPath

But it does not work.

 

Regards!

1 REPLY

Re: Broker in Experiment Manager

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Choroszczynski,
the Experimentmanager cannot set this attribute.
I recommend to use a Variable object of type string as input value containing the Broker path.
You must use the Configuration method (menu Advanced Settings of the Experimentmanager) with the code

root.SingleProc1.imp.BrokerPath := root.Variable.

For the validation you can use Broker1.statMediatedCapacity and Broker2.statMediatedCapacity as additional output values. Maybe you must also the change the Broker path of Exporter and Workerpools in the mentioned Configuration method.
Regards
Peter