Cancel
Showing results for 
Search instead for 
Did you mean: 

Buffer Entrance Lock

Siemens Creator Siemens Creator
Siemens Creator

Hi,

 

I am creating a line that runs two different products in batches along the same process. The process starts with a buffer and I want the buffer to clear of one product before it lets the next product start. I have managed to do this by inserting a single proc before the buffer and locking the buffer entrance when the final product of one batch has left. The problem I now have is that the entrance won't unlock to let the next product through. Does anyone have any ideas how I can do this? I have attached an example of where I am up to so far.

 

Thanks,


Claire

8 REPLIES 8

Re: Buffer Entrance Lock

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Claire,

 

you have to add code to the exit control of the buffer which checks if the buffer runs empty.

 

And when this happen you can open the entrance again.

 

See attached model.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Buffer Entrance Lock

Siemens Creator Siemens Creator
Siemens Creator

That's great, thank you!

 

Just another question, if I increase the capacity on the buffer to the same size as the batch of products I've realised that the method doesn't stop the second parts from entering straight away. For some reason the first part that leaves the buffer doesn't affect the BuffName. Is there a better place to put the method to get the name of the MUs in the buffer to make sure that it won't let any different products in?

 

Thanks,


Claire

Re: Buffer Entrance Lock

Siemens Phenom Siemens Phenom
Siemens Phenom

You can use the pull control of the buffer. This control is called whenever a part tries to enter the buffer. The control can then decide if it allows the part to enter.

Just have a look in the online manual or the examples collection.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Buffer Entrance Lock

Siemens Phenom Siemens Phenom
Siemens Phenom

Attached you can find a model which shows how to use the pull control.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Buffer Entrance Lock

Siemens Creator Siemens Creator
Siemens Creator

That's great, thanks for all your help.

Re: Buffer Entrance Lock

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi All,

 

Building on this initial example, I need to simulate a line instead of a buffer. The logic is similar - let the line process MU of type "a" before accepting MU of type "b" onto the line.

I struggle to get the line going. Can anyone please check what I am doing wrong?

 

Many thanks


Kind regards

 

Irina

Re: Buffer Entrance Lock

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
You need to set minimum gap in the line, so that A can leave, before B starts.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Buffer Entrance Lock

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

working version attached; thanks Steffen!