Cancel
Showing results for 
Search instead for 
Did you mean: 

Buffer or Place Buffer - GAP Zero???

Builder
Builder
is there a way to configurate the Buffer or the Place Buffer to work with Gap Zero? if Not, what object (no length oriented) better represent this application??? Thanks.
2 REPLIES

Betreff: Buffer or Place Buffer - GAP Zero???

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Ricardo,

 

you can use the line, there you can define the gap, the pitch, minimum gap and minimum pitch.

 

Hope this will help

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Buffer or Place Buffer - GAP Zero???

Hi Ricardo,

The "Cycle" object is the tool you are looking for. Here you can choose if you want to have gaps enabled or not.
___________________________________________________________
Friedrich Rutzen, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!