Cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in 13.0.2?

Genius
Genius

Hello,

 

I just installed the update for PS to version 13.0.2 and ran across this issue that I haven't noticed before.

 

I have a Method Control on a Checkbox button with simple code to flip the ?.Value back and forth. I know I've done this in the past without issue, but now when I click on it it looks like the model dumps into an infinite loop. Am I doing something wrong here or is this a bug? 

 

I did find a work around. It seems if I create a new User-Defined Variable and use that in the place of ?.Value it works ok.

 

Best!

Untitled.png

2 REPLIES 2

Re: Bug in 13.0.2?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello EMM,

Nothing has changed here, the model behaves the same in 13.0.0.

When you change the value of the checkbox the control of the checkbox is triggered. Since you change the value in this control it is triggered again, and again,and again, ...

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Bug in 13.0.2?

Genius
Genius

Thanks Ralf. That makes sense now. It's behaving like an observed value. Thanks for clearing this up for me.