Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Bug while opening a read-only tableFile with openDialogBox

Creator
Creator

Hello,

 

I would like to open a TableFile with a method, by using "openDialogBox". 

On the enclosed model, "m_openDialogBox" opens correctly "TableFile" but "m_openDialogBox1" can not open "TableFile1". The only difference between these two tablefiles is that on the second one, the read-only checkbox is set to true.

Can you please have a look at the model.

 

Regards,

Geraldine

 

5 REPLIES 5

Re: Bug while opening a read-only tableFile with openDialogBox

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Geraldine,

 

this is a bug which is already fixed in the maintenance pack 1 (12.0.1).

 

The current maintenance pack is 2 (12.0.2) and we will release maintenance pack 3 in the next few days.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Bug while opening a read-only tableFile with openDialogBox

Creator
Creator
Hello Ralf,

I have downloaded the new pack and it is working well. Thanks.
By the way, do you send a notice each time you release a new pack or a new version?

Regards,
Geraldine

Re: Bug while opening a read-only tableFile with openDialogBox

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Ralf,

 

Not sure if I should have made a new thread but I can't see see patch 3 at all for V12 on GTAC? 12.0.2 is the latest there at the moment.

 

Am I looking in the wrong place?

 

Cheers

 

Ollie

Oliver MacFarlane
Simulation Engineer
web: www.simsol.co.uk
e-mail: oliver.macfarlane@simsol.co.uk

Re: Bug while opening a read-only tableFile with openDialogBox

Siemens Phenom Siemens Phenom
Siemens Phenom

You're right. 12.0.2 is the current one and we post 12.0.3 in the next few days.

I'll correct my posting above.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Bug while opening a read-only tableFile with openDialogBox

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Geraldine,

 

we post it in our Twitter channel which you can reach by clicking on the tile on the startpage.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.