Cancel
Showing results for 
Search instead for 
Did you mean: 

CPU Usage

Pioneer
Pioneer

Dear Community,

 

I'm currently simulating a rather enormeous model, which processes roundabout 90,000 (ninety thousand) MUs.

I would now like to speed up the simulation. Using an Intel Xeon E5 with 4 cores, I noticed that the CPU usage is consistently below 30%.

 

Is there a way to improve the usage of the local CPU?

I'm not trying to use mutliple machines. Also, I already figured out how to allow PS to use all CPU cores via the starting options (or directly using the Task Manager), but so far I was unable to make use of more than 30% of the CPU.

 

Do you have any hints for me?

 

Best regards

 

Tim

1 REPLY

Re: CPU Usage

Siemens Phenom Siemens Phenom
Siemens Phenom

See thread Using-my-whole-processor-cores

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.