Cancel
Showing results for 
Search instead for 
Did you mean: 

Calculating output of singleproc

Valued Contributor
Valued Contributor

I have created a model which consist of line having 7 stages between source and drain. I have 2 duplicate process at second stage whose input I am controlling using Method F20_Input. I want to calculate output of F20 and F20_auxilliary (Single processes) seperately for which I have incorporated 2 different methods F_20_counter and F20_2_counter respectively. After simulating the model for a day I have throughput of 685 and Entity 700 is being transfered on Line after second stage meaning that total of 700 entities have been processed by both F20 and F20_auxilliary. But Using above method I get output of F20 = 533 and output of F20_auxilliary = 540 as shown in image below meaning that total of 1073 output have been processed by both stages which is wrong. Please help me on correcting the method which I have used for counting the output. Also if u can explain about my mistake that will be a great help.

 

Result of Simulation.JPG

PS: I have attached the model below

 

 

2 REPLIES 2
Highlighted

Re: Calculating output of singleproc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have a jam in your line, the exit-control front is called twice, use for the counter rear instead. btw: you don't need to program a counter, each element has his own counter already: statNumout --> check your counter against the value of this attribute

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Calculating output of singleproc

Valued Contributor
Valued Contributor

Thanks...Man Happy

 

It helped me