Cancel
Showing results for 
Search instead for 
Did you mean: 

Calculation of Availability and MTTR

Legend
Legend

Hello,

 

Could anyone advice me how the mean value of the Negexp-distribution for the failure interval is calculated based on Availability and MTTR? I've seen at 50% availability, the mean value of the interval is the same as the entered MTTR.

 

Thank you in advance!

4 REPLIES

Re: Calculation of Availability and MTTR

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Well, that makes perfect sense. The standard approach is sensible in my experience.

 

Basically, if you set an availability you also set an MTTR. Depepending on the MTTR, you need a certain MTBF to achieve the availability. You can easily see it, take 90% availability and MTTR=5 mins, respectively 10 mins. This operation will cut the MTBF in half.

 

Note that the Nex-exp distribution needs only 1 parameter (its mean).

 


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Calculation of Availability and MTTR

Legend
Legend

Thank you for your reply!

 

These are the values I get from changing the availability while having the same MTTR at 60s. The MTBF is the mean parameter in the Negexp distribution for Interval.

 

Availability, MTBF

10, 6.6667

20, 15

30, 25.7143

40, 40

50, 60

60, 90

70, 140

80, 240

90, 540

 

My goal here is to use the same calculation in Excel to be able to show users the effect their entered availability has on the MTBF. But I can't seem to get it to work. 

Betreff: Calculation of Availability and MTTR

Gears Phenom Gears Phenom
Gears Phenom

Well, I get these results with example values:

MTTR [min]AvailabilityMTBF [min]= meanvalue of interval-distribution
1095%190 
1090%90 
1080%40 
1050%10 
1020%2.5 
    
2095%380 
2090%180 
2080%80 
2050%20 
2020%5 

 

I've attached the Excel-file. The basic formula is:

Availability = MTBF / (MTTR + MTBF)

With a little math you can rearrange it:

MTBF =  (Availability * MTTR) / (100% - Availability)

And the MTBF is the mean-value of the failure-duration-distribution.

Does this help?

Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Calculation of Availability and MTTR

Legend
Legend
Yes, that was exactly what I needed, thank you!