Cancel
Showing results for 
Search instead for 
Did you mean: 

Calling a specific failure

Valued Contributor
Valued Contributor

Dear community members,

i have 2 failures types for a SingleProc and I would like to call a specific one with a method. 

More specifically, i want the specific failure to start 240 seconds after the entity enters the SingleProc.

Is it possible?

2 REPLIES

Re: Calling a specific failure

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Alessandro,

 

you cannot activate a specific failure profile.

 

But you can use the methods 'startFailureIn' and 'endFailureIn' to start a failure after a specific time and end it after a specific time.

 

The best is to place these calls in the entrance method.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Calling a specific failure

Valued Contributor
Valued Contributor
Ok, thank you