Cancel
Showing results for 
Search instead for 
Did you mean: 

Can ShiftCalendar handle seconds?

Valued Contributor
Valued Contributor

Is it possible to handle pauses that i not whole minutes long in the ShiftCalendar? Exmple we have pauses that is 45 secunds extra long becose the operators have protective equipment that they need to put on. I have tryed to use format 09:00.45 but plant sim ignore the .45. 

Br Jfinnberg

1 REPLY 1

Re: Can ShiftCalendar handle seconds?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Jfinnberg,

 

the ShiftCalender only supports pauses defined in the time format hh:mm.

 

Kind regards,

 

Igor Kunjavskij

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution