Cancel
Showing results for 
Search instead for 
Did you mean: 

Can a Transporter overtake on a track?

Hi

 

Is it possible that a transporter can overtake on a track? E.g. if a transporter in front are slow or parked for Loading/unloading at a transferStation.

 

Or do some one have a suggestion to a method that can handle it?

2 REPLIES

Re: Can a Transporter overtake on a track?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you could use the collision control of the transporter to "jump over" the transporter (see example).

Or you set up a second track and move the faster transporter temporary to this track for overtaking.

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Can a Transporter overtake on a track?

Some thing like that would also be my best guess if there did not exist a dedicated function for it ;-) Thanks