Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Can't run 3D View

Experimenter
Experimenter

Everytime I try to view or create a 3D model I receive this error and Tecnomatix Plant Simulation 12.1 crashes. I am a new user and not very experienced with the Software. Any help is appreciated. Thank you in advance.

2 REPLIES 2

Re: Can't run 3D View

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Deputyshooter,

 

this is most certainly a problem of your graphics driver.

 

Please make sure that you have the latest version of the graphics driver installed.

 

If this doesn't help go to File->Preference, select the 3D tab and the choose a lower level for OpenGL. E.g. try 3.1.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Can't run 3D View

Experimenter
Experimenter
Hi Ralf

Thanks a lot. I changed the OpenGL level and it worked perfectly fine.

Regards,
Deputyshooter