Cancel
Showing results for 
Search instead for 
Did you mean: 

Can the Viewpoint associated with the camera using Attach MU be manipulated?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

When using Attach [to an object] such as an MU, a fixed viewpoint is defined.

 

Is it possible to manipulte that viewpoint, for example, attach the camera to the MU from its right side, or higher above?

1 REPLY

Re: Can the Viewpoint associated with the camera using Attach MU be manipulated?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Noam!

 

I think that you cannot move camera when attached. However you can change view direction using cursor keys and Shift.

Regards, Vladimir.