Cancel
Showing results for 
Search instead for 
Did you mean: 

Can we purchase 'Fluids' library as an add on..?

Experimenter
Experimenter

Hi,

 

This is more of a commercial question.

We currently use Tecnomatix Plant simulation 10

This version does not come with 'Fluids' libraries so , Can we purchase this library separately?

If so, how do I approach Siememns product team to do this for us.

 

Thanks in advance..

2 REPLIES 2

Re: Can we purchase 'Fluids' library as an add on..?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi VinKam,

 

the fluid objects are available with version 12 of Plant Simulation.

 

They are standard building blocks, not a library.

So it's not possible to use them in an earlier version.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Can we purchase 'Fluids' library as an add on..?

Experimenter
Experimenter

Hi Ralph,

 

Thank you very much for the information...

Appreciate the quick response.

 

Regards,

Vineeth Kamath