Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot Open the Viewer

Legend
Legend

Hello Everyone,

 

I'd like to share my model ( V13.1) thanks to "PackAndGo". 
But when my friend open the model (.exe) he has something like this . He cannot open it. 

I never had this before. Perhaps there is a bug with the 13.1 version ? 

 

Sans titre.png

 

Thank you very much

BR 
OC

 

9 REPLIES 9

Re: Cannot Open the Viewer

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hi,
Make sure you use the same bit versions. If you create the exe on a 64 bit system, it will not run on a 32 bit system. Does the exe work on the machine where you created it?



Verzonden vanaf mijn Samsung-apparaat

Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: Cannot Open the Viewer

Legend
Legend
Hello Nomden,

Thank you for your anwser.
I create the model with the V13.1 and save it (PackAndGo) with the same version.
We all have the 64 bit system.
That's true I can't even open it with my own machine.

Thank you very much
BR
OC

Re: Cannot Open the Viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello ocsim56,

 

I just tested it on a clean install of Windows 7 and it worked without problems?

 

Is this problem related to a specific model or can you reproduce it with a new simple model?

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Cannot Open the Viewer

Legend
Legend
Hello RalfTobel,

Thank you for your answer.
You're right I've just create a simple model with a source and a line. The pack and go worked perfectly.
How come it doesn't work with the other model. That's weird !

Thank you very much
BR
OC

Re: Cannot Open the Viewer

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello OC,
Would be interesting to see what's the problem. Could you open a helpdesk ticket with our support organization or if you don't mind send the model to plantsimulation.studentlicense.plm@siemens.com?
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Cannot Open the Viewer

Legend
Legend

Hello Ralf, 

 

Of course I'll be happy to send my model to the support service in order to have more information about the issue. Actually, I have the professional licence. There is another email adress for the professional users ? 

 

Thank you.
BR

OC

Re: Cannot Open the Viewer

Siemens Phenom Siemens Phenom
Siemens Phenom
No, there is only plantsimulation.studentlicense.plm@siemens.com. Thanks!
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Cannot Open the Viewer

Legend
Legend
Thank you very much.

I'll send it tonight.
Thanks for your help.

BR
O.C

Re: Cannot Open the Viewer

Pioneer
Pioneer
I meet the same problem . do you solve the problem ?