Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot change services exitstrategy carrypartaway

Pioneer
Pioneer

Good afternoon, I have a problem with the assignation of exitstategy servicies with simtalk. I have two workers and when I simulate I obtain the following error.

cannot change services.png

I think it is produced because the code try to change the service of one station while one of the workers has been called before to do the job in that station and because of that Plant simulation can't netiher change the service of the station nor continues reading the code so the error appears.

There is any manner to make the worker called for the singleproc to forget that calling or any other form to let the code change the service without error?

 

Thank you

1 REPLY 1

Re: Cannot change services exitstrategy carrypartaway

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
How do you call this method?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net