Cancel
Showing results for 
Search instead for 
Did you mean: 

Capacity of transporter limited

Experimenter
Experimenter

Hey,

in my PS model I can't change the storage capacity of my transporter. I want it to transport about 200 parts. It's set to store (it neither works with one of the other options) and I though I could change the X- and Y-dimensions to adjust the capacity. Unfortunately the program tells me that I can't change the capacity of my transporter (it also doesn't transport anything when I ignore the warning by changing the dimensions).

Does anyone know a solution to this ?

4 REPLIES

Re: Capacity of transporter limited

Legend
Legend
It's interesting, also my model has the same problem.

A good workaround can be change the capacity by simtalk (Xdim,Ydim).

Re: Capacity of transporter limited

Phenom
Phenom

to me it is not clear,

what is not working as for attached v11 model it seems to work

Re: Capacity of transporter limited

Legend
Legend

You're right, software behaves different only in v12.

It seems a bug, because you see the error message, but after that the attribute "capacity" changes according to data inserted.

Using simtalk everything works.

Re: Capacity of transporter limited

Siemens Phenom Siemens Phenom
Siemens Phenom

The error message is a bug in version 12 and newer. When you see the new capacity in the disabled editfield all should work correctly and the transporter can accept parts up to the new capacity.

The wrong error message will be removed in the next service pack.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.