Cancel
Showing results for 
Search instead for 
Did you mean: 

Carry Away Parts / Assembly depending on Part

Creator
Creator

Hi,

 

I created the attached model where assembly stations assemble on the base of main part type. There are 2 different parts (A and B) to be assembled, at the moment buffers are just linked to assembly stations. I would like instead to use operators and carry away parts, anyway, since assembly depends on main part there's no real target since it can change from time to time. Not sure how to use operators in this case.

 

Thank for your help.

3 REPLIES 3

Re: Carry Away Parts / Assembly depending on Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
they have to carry each single part? Or do they carry a set of parts?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Carry Away Parts / Assembly depending on Part

Creator
Creator

At the moment I'm thinking about single parts.

Re: Carry Away Parts / Assembly depending on Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

this is complicated; in the exit controls of the buffers you need to wait, until the main part is on the assembly station; then you can start the movement of the worker with @.move; if you have more parts to transport, you need to count the parts to transport the right quantity (e.g. using a table).

 

 

Here a short example (only one part).

 

https://www.bangsow.eu/detail_en.php?id=726

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net