Cancel
Showing results for 
Search instead for 
Did you mean: 

Change Frame Background

Pioneer
Pioneer

Good morning.
I have a frame in my project that was built by the former programmer who worked on this project. When I change the background of this frame with an image, the old fund remained and the background that I inserted overlapped, i.e. were the two funds together. Can anyone tell me why? Is there any other way to set the background frame?

 

Sem título2.png

7 REPLIES 7

Re: Change Frame Background

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Martins,

 

in order to investigate the problem I recommend saving the model and loading it.

Can you still see both images?

 

Regards,

Peter

Re: Change Frame Background

Pioneer
Pioneer
Hello Peter.
I saved and loaded the model. The two images will remain.

Re: Change Frame Background

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Martins,

 

for the background in a frame the icon of the frame with name 'Background' is used.

 

Since there can be only one icon with this name, the frame can have only one background image.

 

It's not clear to me from where the other image should come.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Change Frame Background

Pioneer
Pioneer

 

This is the background that is in my model:

 

atual.png

 

This is the image that will be the new fund:

 

Sem título.jpg

 

When I drag the image to the model, rather than just stay the image I dragged both remain:

 

Sem título2.png

Did some testing adding other images, but the first image always remains, only substituting the image I inserted.

 

Follows model attached.

 

Highlighted

Re: Change Frame Background

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is a lot of stuff  created as vector graphics.

 

Activate the vector graphics mode:

vector.png

 

Mark the objects and delete them.

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Change Frame Background

Pioneer
Pioneer
Thank Steffen. I did not know this function of PlantSimulation.

Re: Change Frame Background

Genius
Genius

Hi Martins

 

I can see that your pictures are in poruguese, I'm from Brazil and I can help you in portuguese if you ever need to. Just send me a message and I will be glad to help.