Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Change MU Symbol

Valued Contributor
Valued Contributor

Hi,

 

How can i change the Symbol of an MU ? I have a brick picture for a MU. The MUs will be in a Container and after it passed the printer (SingleProc) I want to change the symbol to a  ColoredBrick. How can I do this ? (model attached)

3 REPLIES 3

Re: Change MU Symbol

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Readock,

 

you can use the attribute 'CurrIconNo' to active another icon.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Change MU Symbol

Valued Contributor
Valued Contributor

I have now a PrintBrick Method and can print a Brick with the code

is
do
    @.setAttribute("CurrIconNo",2);
end;

But how do i print them when they are in the container ?

Re: Change MU Symbol

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

for local i:=1 to @.numMu loop

 @.mu(i).currIconNo:=2;

next;

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net