Cancel
Showing results for 
Search instead for 
Did you mean: 

Change of Anchor Point x & y

Pioneer
Pioneer

Hello,

In previous ver. There was an option to change anchor points x and y manually.

How can you do it in version 12.2.0

achorPoints_x_y.jpg

Thank you

1 REPLY

Re: Change of Anchor Point x & y

Phenom
Phenom

it seems you cannot manually - as in 12.0 - change the anchor points ( column 7..9)  directly.

 

What of course is possible, is to change the anchor points indirectly through column 1 ..5

 

Which would e.g. mean to (re)calculate the target anchor point from tangential angle /length (col 1 ,2).

 

But I think this is a more academic workaround .