Cancel
Showing results for 
Search instead for 
Did you mean: 

Chart: Stacked Columns and Area combined

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Forum

 

I was wondering if it is possible to combine a STacked Columns and Area chart into one simlar to below?:

 

Bar chart and Area.PNG

 

The only solution I can think of is using Annotations but I am curious to see if there are other approaches available?

 

Regards,

Hermias

2 REPLIES 2

Re: Chart: Stacked Columns and Area combined

Siemens Phenom Siemens Phenom
Siemens Phenom

It is not possible to combine different chart types in one chart.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Chart: Stacked Columns and Area combined

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks for the quick reply!