Cancel
Showing results for 
Search instead for 
Did you mean: 

Compare source code of two models with not installed compare program

Siemens Creator Siemens Creator
Siemens Creator

Hello,

 

I use Version 14.2 on Windows 10 and want to compare the soure code (methods) of two models with a not installed Winmerge.

So I copied the folder of Winmerge to the profram files folder "C:\Program Files (x86)" to prevent possible windows security issues.

Then according the help I add the registy key "HKEY_CURRENT_USER\SOFTWARE\Tecnomatix\Tecnomatix Plant Simulation" and add the REG_SZ entry "CompareToolPath" with the value >>    "C:\Program Files (x86)\WinMerge\WinMergeU.exe" "%1" "%2"    <<.
But if I want to compare a method I get the following message box:
Zwischenablage01.jpg

 

Can you help me please what do I wrong?

3 REPLIES 3

Re: Compare source code of two models with not installed compare program

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

the value should be only C:\Program Files (x86)\WinMerge\WinMergeU.exe, as just the path is expected to be passed there.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Compare source code of two models with not installed compare program

Siemens Phenom Siemens Phenom
Siemens Phenom

Try

C:\Program Files (x86)\WinMerge\WinMergeU.exe

instead of

"C:\Program Files (x86)\WinMerge\WinMergeU.exe" "%1" "%2"

.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Compare source code of two models with not installed compare program

Siemens Creator Siemens Creator
Siemens Creator

Is it realy so simple Smiley Embarassed ?  Yes it is. I thought too complicated.Smiley Frustrated

 

Many thanks it works now!!! Smiley LOL