Cancel
Showing results for 
Search instead for 
Did you mean: 

Connect LOCAL Kepware with Plantsim

Valued Contributor
Valued Contributor

Hi All,

 

I'm trying to establish a simple connection between plantsim and a local kepware server.

 

This is in plantsim v12

 

Within the OPC interfaced item, Plantsim is recongnising the server, in that it appears within the dropdown box of the "Server Name" field (see image). If i then tick the "active" box and apply, the OPC item's state changes to a green light.

 

However if i then add try to connect to a tag "Channel1.Device1.Tag10"  The connection then fails. I attached images show screengrabs of plantsim and kepware. The tag is a string and the channel in kepwae is memory based.

 

What is strange is that I had this working a couple of weeks ago and , as far as i'm aware, nothing has changed in my approach/ software settings.

 

Any suggestions would be much appreciated.

 

Shaun

 

 

 

1 REPLY 1

Re: Connect LOCAL Kepware with Plantsim

Valued Contributor
Valued Contributor

I resolved this by uninstalling and re-rinstalling both Kepware and Plantsim