Cancel
Showing results for 
Search instead for 
Did you mean: 

Continuing with the execution of a method , when a another independent method is called

Genius
Genius

Hello Community, 

 

my goal is to continue with the execution of method (x), when another independent method (y) is called. At the moment I am using a user defined attribut (type bollean) which is changed to true, when method (y) is called. With this procedure I am able to continue at a certain point with method (x).

 

My question: I am curious if there is a better way to see with method (x) if method (y) is called? My current procedure is more like a workaround...

 

Thanks in advance! 

3 REPLIES

Re: Continuing with the execution of a method , when a another independent method is called

Phenom
Phenom

What is the specific background for suspending the method(x) ,whilst execution, to wait for another method(y)to start execution ?

Re: Continuing with the execution of a method , when a another independent method is called

Genius
Genius
I am using this to observe if a certain process started, which I am not able to observe otherwise.

In general, I am just curious if there is a way to observe the start of one method with another method.

Something like the following code, which obviously does not exist in this syntax in Plant Sim :

waituntil Method(x).active = true prio1;

Re: Continuing with the execution of a method , when a another independent method is called

Gears Phenom Gears Phenom
Gears Phenom

I agree with @simulator, I don't yet see a need to do what you want to do. Why not split your "waiting" method into 2 methods and the 2nd method is called from the other method?

However, you can waituntil a user-defined attribute turns TRUE, but unfortunately that attribute cannot belong to a method, because then you would have to use the &/ref operator in the waituntil statement. A workaround could be like in the attached example model (specific user-attribute of type boolean for the "other" method, e.g. on a network or on the "waiting" method itself --> then you could use self.~.mFinish_wasCalled).

Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!