Cancel
Showing results for 
Search instead for 
Did you mean: 

Controlling MU Flow from Multiple Lines on to one line with sensors and Methods

Pioneer
Pioneer

Hello

I have a simulation that has 4 lines that feed in to a single line, this is controlled by sensors at the end of each line and only one MU can enter the end line I am just wondering how program a method to stop and start the Lines depending on the signals of each sensor and how I reference the Sensor from each Line in the same method

Thank you for the help

1 REPLY 1

Re: Controlling MU Flow from Multiple Lines on to one line with sensors and Methods

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Gareth_Henry,

 

a sensor control has two parameters. The first is the sensor id and the second tells you if the sensor was triggered by the front or back of an MU.

 

The '?' gives you access to the caller of the sensor contro, i.e. the line on which the sensor is located.

 

Using these values you can identify the line and the sensor.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.