Cancel
Showing results for 
Search instead for 
Did you mean: 

Controlling line flow with sensors

Experimenter
Experimenter

Hello, i'm having problems trying to simulating this case: I'm using a conveyor with sensors to simulate operations in a line, when the sensor detect de MU it will stop certain time, the sensor will get the time from a table file; Currently im using line.stopped in the method but the problem is that when the sensor detect de MU all the line stop but i want to stop only that MU not all the line.

I'm attaching the simulation.

 

Thanks

 

Regards

3 REPLIES 3
Highlighted

Re: Controlling line flow with sensors

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
is this the right file?

A line you can only stop completely, so you need to split the line into segments and stop the segment.
Another way is to model the parts as transporter, the line as track. Then you can stop the parts (as transporter).
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Controlling line flow with sensors

Experimenter
Experimenter

Hello, sorry i attach the wrong one, already added the correct one.

i will try split the line in segments; thanks

 

Regards

Re: Controlling line flow with sensors

Siemens Phenom Siemens Phenom
Siemens Phenom

@.stopped:=true --will stop the MU on line or track, nevertheless what kind it is (Entity, Container, Transporter)

wait MyTime

@.stopped:=false --will release the MU

 


Regards

Always consider using the AttributeExplorer!