Cancel
Showing results for 
Search instead for 
Did you mean: 

Converter Capacity

Legend
Legend

Hello everyone, 

What is the simplest way to impose a capacity of the Converter. 

I'm trying to handle it thanks to an entrance method and the EntranceLocked (of the converter), in order to have only one MUs on the Converter at a time. This works well but sometimes I notice two MUs on the same converter, as you can see on the picture below.

 

Thank you very much. 

BR 
O.C
converter_capacity.png 

 

8 REPLIES 8
Highlighted

Re: Converter Capacity

Phenom
Phenom

Hello

 

Have you tried the capacity field of the object? By default it will be -1 which is as many as will fit but if you change it to 1 then only 1 mu should be allowed on at a time.

 

JamesM

Re: Converter Capacity

Legend
Legend
Hello James,

Thank you for your comment.
I can't see any Capacity Field in the Converter object, do you ?
I'm using 12.0.5 version.
Thanks

Re: Converter Capacity

Phenom
Phenom

Have just checked the 2 versions that I have got (12.1.1 and 12.2.1) and both of them have got the capacity field on the main tab of the dialog that opens for the converter.

Re: Converter Capacity

Legend
Legend

In the version I have the converter main tab looks like this : 

converter_capacity.png

I'll try to set up 12.1 version and I'll keep you in touch. Thank you James ! 

Re: Converter Capacity

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
it is missing in the version 12.0..., but you can set it directly in the attributes and method window (F8), double click on the line capacity and set the value
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Converter Capacity

Phenom
Phenom

Thanks Steffen_B, that was going to be the next thing I was going to suggest but you beat me to it.

Re: Converter Capacity

Legend
Legend
Steffen,

I already tried this trick in vain !
I got an error "Cannot change capacity" !

Thanks

Re: Converter Capacity

Legend
Legend

I updated the software to 12.2. 
It works well we can modify the converter capacity ! 

 

Thank you very much ! 

Regards 

O.C