Cancel
Showing results for 
Search instead for 
Did you mean: 

Copy statistics from old to new BE

Creator
Creator

Hello everybody,

 

My problem is the following:

After a BE has been edited in a single station, I would like to replace it with another BE, but copy the statistics of the old BE on the new BE. I have started to realize this via the output control (bug) of my single station. It is also important that the new BE is generated directly in the output area of the single station, so that it won't activate the output control again.
Does anyone have a solution for this?

 

Thanks and best regards,

Robert

3 REPLIES

Re: Copy statistics from old to new BE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the new created part will trigger the exitcontrol again; a simple solution is to rename the MU and to change the icon in the exit control rear
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Copy statistics from old to new BE

Creator
Creator

Thanks for the help!

However the new BE would have a bunch of new attribute and therefor its inevitable to use it.

Maybe the activation of the exit control is not that crutial. More important is to awoid another processing of the new BE.

 

Is there a way to realize that?

 

Re: Copy statistics from old to new BE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
have a look into the help: method create --> the created MU is immediately ready for exit
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net