Cancel
Showing results for 
Search instead for 
Did you mean: 

Copy the model

Builder
Builder

hello,

 

Is there any feature in plant simulation where we can copy a line or model in the same frame.Suppose there is three same assembly line in the frame,so is it possible to make model of one line and then copy it two times,so that we dont have to model same thing three time????

1 REPLY 1
Highlighted

Re: Copy the model

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello k_parashar,

 

just mark the objects you want to duplicate and then press Ctrl-C to copy them into the Clipboard. Now you can insert them with Ctrl-V as many times as you need.

 

But please consider creating a class in the class library which you then also can insert as many times you want.

The advantage you then have is the inheritance of the structure and attributes.

So if all instances should be changed you just have to change the class.

 

Rregards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.