Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Core usage strategy

Legend
Legend

Hello,
I'm wondering what happens exactly when I run several models altogheter.
If I use the experiment manager with distributed simulation activated I can use every core of my machine.
Happens the same opening different instances of plant simulation  (so without using the experiment manager)?

Regards
Alessio

2 REPLIES 2

Re: Core usage strategy

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes of course.

Multiple instances of an application means different processes for the scheduler of the operating system. They will be distributed to different CPU cores.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Core usage strategy

Legend
Legend

Thank you