Cancel
Showing results for 
Search instead for 
Did you mean: 

Crane Error

Valued Contributor
Valued Contributor

Good afternoon.
I upgraded the version of Plant Simulation from version 13.2 to 14.
When I went to execute a project an error occurred in the crane.
The error occurs constantly during execution.
What can it be?

error crane.png

 

 

 

3 REPLIES 3

Re: Crane Error

Phenom
Phenom

Well, according to the detailed message , the crane cannot reach the (target) position.

 

Without having a look at the model/ sub model it will turn out to a guessing, what is causing this message.

Re: Crane Error

Valued Contributor
Valued Contributor
Despite the detailed message, it is an error that never occurred before and there was no solution in the forum. A problem actually resulting from a point beyond the reach of the bridge, but at an almost imperceptible distance. The error did not occur in versions earlier than 14 because the object was teleported.
Highlighted

Re: Crane Error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Henrique,

 

this is not an error, it is a message telling you that the target position of the crane cannot be reached.

 

In earlier version the crane remains at his position and throws the part to the target station. This was a bug.

 

Can you please provide your model so that I can examine the message in more detail?

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution