Cancel
Showing results for 
Search instead for 
Did you mean: 

[Crash] Right clicking in gray area of an objects contentslist crashes Plant Simulation

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

I am running Plant Simulation V14.1, but the bug seems to be present all the way back to Plant Simulation V12.

 

There seems to be a bug where right clicking in an object's contentslist area (the gray part) creates a program crash.

 

This seems to be the case for all objects which can contain other objects, in other words where a contentslist can be accessed (singleproc, buffer, assemblystation, container, etc.).

 

Steps:

 

1. Open an object with double click (for example a Container in .MUs.Container)

2. Press Shift + F8 or go to "View -> Contents". A new dialog with the object's contents should be shown.

3. Right click in the gray area inside this window (outside the table cells) --> Plant Simulation instantly crashes.

 

image.png

1 REPLY 1

Re: [Crash] Right clicking in gray area of an objects contentslist crashes Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

thank you very much for pointing this out, the issue will be fixed with the next maintenance pack.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution