Cancel
Showing results for 
Search instead for 
Did you mean: 

Create connector between 2 frames via simtalk

Builder
Builder

Hi all,

 

I have 2 frames in my model and I need to createvia simtalk a connector between the 2 frames. How is it possible ?

Should I do a createobject, and then manually type all the attributes ? Which attributes of the connectors and the frames do I look for ?

 

thanks in advance !

 

Flo_M

7 REPLIES

Re: Create connector between 2 frames via simtalk

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Flo_M,

 

just have a look in the online manual at the 'connect' method of the Connector object.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Create connector between 2 frames via simtalk

Builder
Builder

Exactly what I needed !

 

Thanks !

Re: Create connector between 2 frames via simtalk

Creator
Creator

Hi,

 

I would like to ask if is it possible to create a connector via SimTalk to connect a line to a Transporter. As I have an application in which I require to move a part from a line to a transporter smoothly. I do not wish to use move, transfer or insert instructions as it make the animation rough. I need a smooth movement.

 

Thanks

Re: Create connector between 2 frames via simtalk

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You cannot connect a transporter with a connector. The key for your "smooth" loading is the loadbay-type line in connection with move. Move moves the MU only to the start of the next element (loadbay of the transporter). Then the transporter transports the part until the end of the loadbay. If your animation is rough, then you need to adjust the animation on the transporter and the number of amination events.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Create connector between 2 frames via simtalk

Creator
Creator

Thanks.

 

I have Technomatix version 10.1. The model you attached does not open. Would you be able to make it compatible for me?

 

Thanks

Re: Create connector between 2 frames via simtalk

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

here is the example in 10.1

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Create connector between 2 frames via simtalk

Creator
Creator

Thank you very much.