Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Create new model on startup

Legend
Legend

Hello!

 

I'm trying to create a new model when starting the program. I haven't found any command line arguments to do this. The closest I've come is to use -lib: without an argument. That makes the program start a new model but ignores all other command line arguments unfortunately.

 

The arguments for -lib are SDX and AMG, I think it would be great to be able to specify a library name here which would open a library available from the "Manage Class Libraries" dialogue if found. I.e, also including user-specified additional libraries.

 

Either that or being able to just start a new model as a command line parameter.

 

Anyone having this problem as well or think it would be a good idea?

2 REPLIES 2

Re: Create new model on startup

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Verbalins,

Why not just save a blank model, let's say as a template, and then just load it?

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Create new model on startup

Legend
Legend
Hello Ralf,
thank you for your response.

Yes, that is how I'm doing it currently. I was just thinking if it was possible to do it in another way to reduce the number of files needed. Maybe I will use the COM-Interface instead.