Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating / Deleting Animatable Objects via SimTalk

Phenom
Phenom

Hello all.

 

Another 3D question here, is there a way to create or delete an animatable object through code?

 

I have searched the help system and cannot find a way to do so apart from using the interface, and have been trying to find all of the different attributes and methods that can be used with it (from the ._3D.GetObject(String/Integer) method).

 

JamesM

3 REPLIES

Re: Creating / Deleting Animatable Objects via SimTalk

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm afraid, there is no such SimTalk function in any released version of Plant Simulation. However, Plant Simulation 13.1 will have one.

Re: Creating / Deleting Animatable Objects via SimTalk

Phenom
Phenom

Hello.

 

Thank you for the quick reply. Guess I will have to wait for 13.1 to do that then.

 

JamesM

Re: Creating / Deleting Animatable Objects via SimTalk

Phenom
Phenom

Hello.

 

Can confirm that the methods have been added and works well.

 

JamesM