Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating Failures via Simtalk

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello All,

 

I am trying to create a failure across a few stations utilizing SimTalk. 

 

I am using a dialog box to retrieve the Name, Availability, and MTTR of a failure. I am then storing the name in a variable and creating a failure off of the information provided.

 

The problem I am having is that the variable cannot be used in an assignment statement for Availability or MTTR.

 

See the following code below:

 

tempName := FailureDialog.getValue("NameEditBox");

Station1.Failures.createFailure(tempName);

Station1.Failures.tempName.Availability := 95.00;

Station1.Failures.tempName.MTTR := str_to_time("1:00:00");

 

This code does not work as I get an error for an Unknown identifier for Failures.tempName.

 

Is there a way to assign Availability and MTTR to a specific failure in simtalk?

 

Thank you!

3 REPLIES 3

Re: Creating Failures via Simtalk

Siemens Phenom Siemens Phenom
Siemens Phenom

Station1.Failures.tempName addresses a Failure named "tempName". If the local variable 'tempName' contains the string "abc", you would have to write Station1.Failures.abc instead. So for your code to work, you first have to retrieve the just created failure like this:

local tempName : string := FailureDialog.getValue("NameEditBox");
Station1.Failures.createFailure(tempName);
local f := Station1.Failures.getFailure(tempName);

f.Availability := 95.00;
f.MTTR := str_to_time("1:00:00");
_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Creating Failures via Simtalk

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you Michael!

 

That worked perfectly. 

 

Now, I have one more question:

 

I have this code in my reset method and so if I click reset twice, I get the error that the name already exists in the name scope of the object. This is because it is trying to create the same failure again. Is there an if statement or something that can ignore the createFailure call if the failure name already exists?

 

Thank you in advance!

Re: Creating Failures via Simtalk

Phenom
Phenom

have you tried

if Station1.Failures.getFailure("failureName") = VOID then
	Station1.Failures.createFailure("failureName");
.
.
. end;