Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating container with MUs using source

Hello,

 

normally the object source create MUs like entity, container etc; there is a way to create, with source only, a container with one entity inside without using assembly station?

Thank you

 

3 REPLIES 3

Re: Creating container with MUs using source

Genius
Genius

I dont think so, but you could embed them in a Frame so that it looks like one object. If you went through the beginner tutorial (in the help) you should be familar with how to do this.

 

Untitled.png

 

Re: Creating container with MUs using source

Phenom
Phenom

you also have the possibility to create a MU in the container on the source through

the "create" method.

Unbenannt.png

 

 

Re: Creating container with MUs using source

Genius
Genius

lol. yeah, this would be much simpler. do that ;-)