Cancel
Showing results for 
Search instead for 
Did you mean: 

Cross Sliding Car -- BUG when using Drag & Drop

Genius
Genius

Hello everybody,

 

I have a problem with the object cross sliding car (version 13.2). In the attached screenshot you can see a message which appears, if I want to connect with drag & drop an object of type Track with the object cross sliding car. The object Track, which I want to connect with the cross sliding car, is a derivation of an object defined in my class library. This object has an own exit control. But Plant Simulation changes automatically the exit control to self.OnExit, after I connected the derivation of the object track with the cross sliding car. This should not happen.Unfortunately the source code of the cross sliding car is encrypted Smiley Sad

 

Do you have an idea how I can solve this problem?

 

 

Thanks in advance!

Niels

 

Schiebebuehne_Bug.PNG

5 REPLIES 5

Betreff: Cross Sliding Car -- BUG when using Drag & Drop

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Niroe,

 

as you can read in the error message, there is an invalid identifier. Can you please provide your model so that we can analyze the error message in more detail.

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Cross Sliding Car -- BUG when using Drag & Drop

Genius
Genius

Hello GG,

 

thank you for your answer. Unfortunatley I cannot send you the original version. But I created an example. Please find it attached. It show the same error. My goal is, that the exit control "self.test" will be not automatically replaced by Plant Simulation with "self.OnExit".

 

Please try to connect (drag & drop) both tracks with the cross sliding car. And afterwards have a look for the exit control

 

Thanks again!

 

 

Betreff: Cross Sliding Car -- BUG when using Drag & Drop

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Niroe,

 

you are using an old version of the library.

The bug is already fixed. Attached you will find the current version of the library.

Hope this helps.

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Cross Sliding Car -- BUG when using Drag & Drop

Genius
Genius

Thank you GG!

 

The new version of the cross sliding car works perfect!

 

One more question: Is there a way to change the symbol of the car ?

 

Thanks & enjoy your weekend!

Niels

Betreff: Cross Sliding Car -- BUG when using Drag & Drop

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Niels,

 

the icon of the CSC in 2D is automatically created by Plant Simulation.

The 3D geomatry is created by method.

In current version, both representations cannot be modified.

Sorry for that answer.

We will think about customizing the graphic of the CSC, but only in 3D.

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution