Cancel
Showing results for 
Search instead for 
Did you mean: 

CrossSlidingCar 2 cars on one system

Pioneer
Pioneer

Hello, Plant community Smiley Happy

 

I have been working on one problem and was using CrossSlidingCar, but in real system there are 2 Cars on one rail (and they cannot collide between each others - obvious Smiley Happy )

Now I put one CrossSlidingCar and then one more CrossSlidingCar on top of that. And they go trough each others. Do any of you know how to build a logic that they do not collide or how to put 2 cars on one rail?

 

thanks and regards

3 REPLIES 3

Re: CrossSlidingCar 2 cars on one system

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi HugoZupan,

the library CrossSlidingCar does not support multiple vehicles. But there is a Crane library for multiple cranes on a single rail. This example shows a way to realize such a control. Please look at the Example Collection, which can be opened via the

Start Page: Example Models > Small Examples > Category: Continuous material flow > Topic: Portal crane > Crane with 2 Portals.

Regards,

Peter

 Portalcrane.gif

Re: CrossSlidingCar 2 cars on one system

Legend
Legend

Hi,

I had the same problem.
If you are handy with simtalk I suggest to create by yourself the object you need using distance and collision control.

Re: CrossSlidingCar 2 cars on one system

Siemens Phenom Siemens Phenom
Siemens Phenom

The attribute TargetPosition of the Transporter will also help you.