Cancel
Showing results for 
Search instead for 
Did you mean: 

.DWG as 3d background

Pioneer
Pioneer

Hello, is there a way to use a .dwg file as a background on a 3d frame? I'm using it on 2d, but i also want it to be on 3d as the "floor" of the plant.

Thanks

4 REPLIES

Re: .DWG as 3d background

Phenom
Phenom

either convert the dwg-file to vrml and import it to 3D

 

or create a bitmap format ( e.g. bmp /git/tif/jpg) and add it as a texture to a textured plate

Re: .DWG as 3d background

Siemens Phenom Siemens Phenom
Siemens Phenom

In 12.2 you can import a DWG file into 3D or drag it onto a 3D window and it will automatically create a textured plate for you.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: .DWG as 3d background

Pioneer
Pioneer

I'm using the 11, do you know if there is a way to do that in it?

I tried the suggestions above but none of them worked :/

Re: .DWG as 3d background

Phenom
Phenom

What do you exactly mean by "doesn't work" ?

 

s. below  screenshot of a textured plate with an added jpg

 

VRML2 import works as well

 

xxx.png