Cancel
Showing results for 
Search instead for 
Did you mean: 

Date drop down selection from calendar

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi forum

 

I want to use a dialog to insert project start dates and end dates.

currently I have it like the picture below:

Calendar Dialogbox.JPG

What I would like to do is change the Date inputs to select from a drop-down calendar like you get in windows:

date selection.JPG

 

I know it is possible and probably quite simple but I am not sure where to look for the simtalk required.

Any feedback will be much appreciated!

 

Regards,

Hermias

3 REPLIES 3

Re: Date drop down selection from calendar

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hermias,

 

It used to work through ActiveX, using the MSCAL.Calendar.7 class. But this functionality was dropped/replaced by Microsoft.

 


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Betreff: Date drop down selection from calendar

Gears Phenom Gears Phenom
Gears Phenom

Hi Hermias,

 

some time ago I wanted to have the same thing and built myself a dialog inside Plant Simulation, that offers the same functionality like the Windows dialog:

 

Screenshot - 22_04.png

 

It works fine, but it was a lot more work than anticipated (and now it is not even used...)!!

 

Since I did this during my work, I cannot "give away" the tool, but if you want some information/tips on how to re-build my tool, I'll try to help you.

 

Best Regards,

Alex

 

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Date drop down selection from calendar

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks for the feedback Alex.
If it becomes a vital requirement I'll definitely get in contact with you.

Regards,
Hermias