Cancel
Showing results for 
Search instead for 
Did you mean: 

Deactivating sensors

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello guys,

 

Is it possible to deactivate the sensor on the track/line and keep it on the line at the same time? I dont want to use destination so I basicly set FRONT and REAR to False and its deactivated the sensor. 

 

Is there any other way to deactivate sensor ?

 

Thanks !

2 REPLIES 2

Re: Deactivating sensors

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

There are some options. When using sensors, of course in the very beginning of your sensor control method, you could program a condition check and use the return command immediately if the required conditions are not met at a specific sensor.

 

Alternatively, in the latest versions you can also choose to set the attribute TargetPosition to send a Transporter to a specific position on a track onto which the Transporter is located. This only works for Transporters on Tracks.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Deactivating sensors

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thank you for your answer and advice Nomden. I like the idea of using Return command when the required conditions are not met.