Cancel
Showing results for 
Search instead for 
Did you mean: 

Debuginfo to variable

Pioneer
Pioneer

Dear all,

 

I'm currently exploring the possibilities of analyzing the performance of my simulation model.

In this context, I wondered if and if yes how it is possible to access the DebugInfo directly, such as writing the CPU Time, Events per second etc. directly to a table?

 

I do believe it would be possible to redirect the console output to a file and read from that file, but I can't really believe this should be the only way. Is there a possibility of directly accessing these infos?

 

Best regards

 

Tim

1 REPLY 1

Re: Debuginfo to variable

Legend
Legend

Please check Activate Profiler in the Help menu. I hope it helps you. 

 

in the debugger menu "activate profiler" everytime you run the model. Once activated it will give you model analytics by clicking "Show profile". 

Capture.JPG

 

 

 

 

 

Sachin