07-05-2017 05:31 AM
07-05-2017 07:16 AM
apart from that I don't think it is possible -
why do you want to delete
an event from the eventlist ?
07-05-2017 09:05 AM
Hello thanks for the reply
I find a way to solve the problem without delete event in Eventcontroller
I also think that it is not possible to delete event
So I try the block the generation of event instead of delete it after the event is generated