Cancel
Showing results for 
Search instead for 
Did you mean: 

Demand for a "!==" functionality

Builder
Builder

Hi!

 

There is a functionality "==" existing in PlantSimulation to compare two values being regareded as equal according to a given parameterized boundary.

 

But there is no "definitely unequal" functionality like "!==", to ensure, that two values are outside of that boundary.

 

If I am using smaller "<" or larger ">" it returns true even when the difference is (invisible) small.

 

Can this be added?

3 REPLIES 3

Re: Demand for a "!==" functionality

Phenom
Phenom

Hello.

 

/= is not equal to.

 

JamesM

Re: Demand for a "!==" functionality

Builder
Builder

Please, first reading THEN THINKING ...

... and then probably answering.

 

What do you want me to do with the following:

 

Rubbish!.jpg

 

To clarify: I wanted to have something that returns true when "==" is not fulfilled, which means there is a difference between two values that exceeds the numerical rounding errors covered by "==".

Re: Demand for a "!==" functionality

Phenom
Phenom

Ok then.

 

not (result == bestResult)

 

JamesM