Cancel
Showing results for 
Search instead for 
Did you mean: 

Diagram Plant Simulation 12 on Win 8.1

Pioneer
Pioneer

Hi,

i have tried the new version Plant Simulation 12.0.1 with some standard models.

Unfortunately the Diagram Object doesn't work. It is only showing a black window like in the attached screenshot.

In Plant Simulation 11 TR2 it is working perfectly right on my computer.

Im am using Windows 8.1 64 and the Plant Sim 12.0.1 x64.

 

Has anyone the same problem, or knows what i need to do?

 

Thank you for your Help

4 REPLIES 4

Re: Diagram Plant Simulation 12 on Win 8.1

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi HS_Kempten,

 

we had this problem once. The reason was related to the energy saving settings in Windows.

 

Can you try to set the power settings in the control panel to High Performance?

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Diagram Plant Simulation 12 on Win 8.1

Pioneer
Pioneer

Thank you for your quick answer.

I set the power settings on high performance, but i can still only see the black screen.

 

Regards

Martin

Re: Diagram Plant Simulation 12 on Win 8.1

Siemens Phenom Siemens Phenom
Siemens Phenom

We actually do not know why the Power Options affect the chart at all. It might have something to do with the graphics card driver.

 

I would suggest that you try out all available power plans, including the ones in "additional plans". You may need to expand the "additional plans" first.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Diagram Plant Simulation 12 on Win 8.1

Pioneer
Pioneer

The Problem with the "blacked" Diagram does not occure with the new Patch 12.0.2 anymore.

Thank you for solving this so quickly.

 

Regards