Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Dialog as User Interface, how to write variables

Legend
Legend

Hi all,

 

I like to create a dialog page to allow the model user (in run time use) to turn on/off checkboxes, enter parameters etc...

Now don't see how I can do this.

- Is it possible to directly put and write to variables to the dialog which are located on the Frame ?

- The callback method can not be changed (is read only). If the above request can not be implemented, I need to have additional checkboxes and variables in the dialog and copy these to the variables in the frame or tablefile etc...

I guess the operator should change the variables on the dialog and press the 'Apply' button. This would trigger the Apply code in the callback method.

 

I went through Stefan B's document section 2.14.

I attached a simple example where I like to us the dialog window variables to update the variables on the Frame.

 

 

Kind regards

Marco

2 REPLIES 2

Re: Dialog as User Interface, how to write variables

Legend
Legend

...forgot the file

Re: Dialog as User Interface, how to write variables

Legend
Legend

I spend some time on this and found out how it works.

 

The callback method which is in the Dialog has to be replaced by a new one, copying its content and adding the required own code to copy the variables between the Dialog and Frame variables.

This is either intended by Siemens or a mistake.

Creating an observer I get a method with the interface. I can change this code.

 

The key is the "setvalue" and "getvalue" command.

 

Attached is an updated model show how to do.