Cancel
Showing results for 
Search instead for 
Did you mean: 

Dialog inside the frame does not open on double click !!!!

Hello Community,,

 

I am trying to use dialog box inmy frame and want to open the dialog window when i click on the frame from outside.

I tried everything but it is not happening. I have given a open control method but when i click the frame instead of opening the dialog it goes inside the fram.

May be i am missing a key step here.

Any help will be appreciated??

6 REPLIES 6

Re: Dialog inside the frame does not open on double click !!!!

Siemens Phenom Siemens Phenom
Siemens Phenom

Did you enter the open control in the Frame or in the Dialog?

It is important that you enter it in the Frame!

 

By the way: You can enter the Dialog instead of the Method into the open control.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Dialog inside the frame does not open on double click !!!!

yes!! I have written a method inside the frame

Tha name of method is : open_control

content is : dialog.open

 

can you see some error ?

Re: Dialog inside the frame does not open on double click !!!!

Siemens Phenom Siemens Phenom
Siemens Phenom

Make sure that no object inside the Frame window is selected. Then click on the "Controls" button in the ribbon bar. Check that the window title shows the path to the Frame. Then enter the Method or the Dialog.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Dialog inside the frame does not open on double click !!!!

you mean the controls button in debugger ribbon tab ?

Re: Dialog inside the frame does not open on double click !!!!

I found it and its working. Thank you!!

Re: Dialog inside the frame does not open on double click !!!!

Siemens Phenom Siemens Phenom
Siemens Phenom
please accept the solution in order to help others too ...


Regards

Always consider using the AttributeExplorer!